Here's a quick tutorial video about your Lyo-Works Operating System.
Watch: LyoWorks Operating System
The OS should fully load within about 90 seconds after you plug in your FreeZone Freeze Dryer and wait for the screen to illuminate.
Once the loading screen animation has ended, the main menu, collector temperature and the vacuum level are displayed, and the current operational mode will be displayed: manual, standby or defrost. The main menu icons populate the top of the screen, and text-buttons along the bottom of the display allow you to switch between auto or manual mode. You will also access settings for any accessories or options that have been added to your FreeZone Freeze Dryer using buttons that will appear along the bottom of the home screen.
This video also details how to add and edit programs and program parameters, and describes how to set up, start and stop data logging. Learn how to chart data onscreen and how to export data. Additional advanced features can be accessed when your FreeZone is connected to the internet via its ethernet port.
For complete details on Lyo-Works OS feature settings, view the tutorial video.