Skip to main content
Science Center on Science Hill – Wellesley College

Wellesley - Science Center on Science Hill - Labconco

On August 20, 2024

Science Center - Wellesley

While the construction of the L-wing of the new Science Center began in the summer of 2018, the college moved the teaching labs into modular buildings. Low ceiling heights in the temporary space created a challenge, but with Wellesley’s strong interest in green, energy efficient technologies, Echo Filtered Fume Hoods were an ideal fit.

fume-hood-journey
flex spaces

The L-Wing Renovation allowed for more natural light and collaborative lab spaces. Once the new wing was complete, the filtered fume hoods were moved to their new locations inside the Science Center. Smart planning allowed many of the hoods to find appropriate spaces in both the flex labs and the permanent labs, and saved the college nearly two hundred thousand dollars a year in energy and maintenance savings.

Installation: Apr, 2019

view-of-hall
ducted-and-filtered

Challenge

on. Temporary buildings, however, cannot be fitted with the same level of controlled airflow equipment that's required for the traditional fume hoods.

Working with chemicals generally creates safety complications. The solution to handling fumes within a building is to incorporate motorized blowers to draw fumes out of the building, which in turn creates a need for a certain number of air changes per hour and a safe amount of supply air to make up for the air being exhausted from the building. These demands culminate in a complicated mechanical system that would be inappropriate for a temporary space.

Later, in the permanent building, more demonstration and lab work space was required to accommodate the increasing number of science students. The increased energy demand of adding a number of fume hoods was a consideration, as well as the physical impossibility of providing the required make-up air for the number of hoods required.

filtered-boards
side-by-side2

Solution

Since ducting out of the temporary spaces was not an option, Echo Filtered Fume Hoods were used to retain as much flexibility as possible. Traditional ductless hoods use filters that are optimized to handle a specific range of chemicals, which doesn’t work well in a teaching lab that may encounter a wide range of applications. Echo Filtered Fume Hoods, on the other hand, use patented Neutrodine Unisorb filters, which can handle a broader range of chemicals than other carbon filters, including limited levels of solvents and even acids.

Benefits

Since Echo Filtered Fume Hoods don’t make any demand on the mechanical system, it was possible to maximize the number of hoods per student, providing more hands-on teaching spaces to work with chemicals, vapors and dusty materials.

The energy savings per hood was dramatically increased since the filtered hoods consume less than 1% of the energy demanded by ducted hoods. Wellesley managed to avoid the difficulty of increasing the operational costs by using filtered hoods.

Assuming $5000 in savings each year (See “Cost Comparison: Budgeting for a Filtered Fume Hood” below), 39 Echo Filtered Hoods will generate inf $195,000 per year in energy and maintenance savings. For the 20 year expected lifetime of the building, that’s $3.9 million in savings.

Cost Comparison: Budgeting for a Filtered Fume Hood