Skip to main content
building-emitting-dollars.jpg

Zero Net Energy (ZNE) lab uses filtered fume hoods

On May 7, 2015
Posted in Case Studies

Laboratories are notorious for being energy hogs. The expense of heating and cooling the air that is exhausted out of a lab to provide scientists a safe working environment is one of the biggest expenses a lab incurs.

By using filtered fume hoods, the number of air exchanges in a lab can be drastically reduced. Because filter technology has evolved over the years, a larger variety of applications can be performed safely in a filtered hood.

Read about the use of Filtered Fume Hoods at Bristol Community College and other design features in the new Zero Net Energy (ZNE) lab: “The 50,000-sf New Technology and Learning Center (NTLC) for Bristol Community College (BCC), Fall River, Mass has achieved what was considered unthinkable just a few years ago, a Zero Net Energy Laboratory.”