Skip to main content
echo-without-model-1000.jpg

How can a Filtered Fume Hood free up my lab's budget?

On August 26, 2015
Posted in Articles

On-Demand Webinar: Spending a Fortune with Ducted Fume Hoods? - Safe Alternatives to the Traditional Ducted Fume Hood

Link

Unlike ducted hoods, Filtered Fume Hoods do not exhaust your laboratory’s costly tempered air to the outdoors. People are often surprised to learn that the annual energy savings gained by switching to Filtered Fume Hoods pays for the switch many times over the life of the hood.

The greatest savings are due to completely eliminating the cost of make-up air. Filtered Fume Hoods also eliminate the need to emit pollutants into the atmosphere. The most advanced filter for this type of hood is the Neutrodine™ filter, which is composed of plant-based carbon materials and impregnated with neutral non-toxic agents. Once expended, Neutrodine filters may be incinerated for environmentally-safe disposal.

The following Cost Comparison Chart shows how the lower operating costs of a filtered hood compare to a traditional ducted hood in various configurations.

Echo Filtered Hood savings chart

If you're ready to see if a filtered fume hood will work for your application, the first step is to request a Chemical Assessment.

**Labconco icon 75h

Request Chemical Assessment**