Support Shelves attach easily without tools to the sides of the FreeZone 1, 2.5 or 4.5 Liter Freeze Dryer or left-hand side of the FreeZone Triad Freeze Dryer cabinet to provide support for large flasks attached to the drying chamber or manifold.
Multiple rows of perforations on the sides of the FreeZone cabinet allow for height adjustment of the shelves to support various sizes of flasks. One pair. Glacier white epoxy-coated steel wire.
May also be used in side storage compartment of FlaskScrubber Vantage washers manufactured after October 2020 to hold small supplies such as Printer 4681301.