Lab & Science News

Infographics

Infographics 03-28-2017

Infographic: lyophilization, concentration or evaporation, which is best for my samples?

This infographic will help you select the right methods and equipment to best preserve your specific samples. Lyophilization, concentration and evaporation (including nitrogen blowdown) methods are all considered. 

Infographics 03-07-2017

Infographic: Selecting USP 800 Equipment

This infographic will help you understand how to select the right solution for USP <800> in your pharmacy...

Infographics 01-24-2017

Infographic: How to Select a Fume Hood Blower

Select a blower that's designed and manufactured for superior performance and long life when subjected to chemical atmospheres. Blowers are available in sizes that can handle airflow as low as 250 CFM, to blowers that can handle airflow as high as 3500 CFM... 

Infographics 11-08-2016

Infographic: Fume Hood Operation DO's & DON'Ts

Keeping you safe in your laboratory is what we think about every day, so we developed this infographic along with Lab Manager Magazine to help you work safely in your laboratory's fume hoods...

Infographics 07-26-2016

Infographic: How to Select the Right CA Fuming Chamber

Cyanoacrylate (CA) or superglue fuming has been a mainstay for forensic scientists for decades. Developed in Japan, this procedure for fixing latent prints has been adopted worldwide. We're proud to support forensic scientists everywhere with our forensic line of equipment.

Infographics 05-25-2016

Infographic: SEFA 9-2010 Ductless Enclosure Classifications

The Scientific Equipment and Furniture Association (SEFA) is an international trade association that aims to improve the quality, safety and timely completion of laboratory facilities. To streamline these processes, ductless enclosures are currently classified into three categories...

Infographics 03-25-2016

Infographic: How to Select a Glove Box

Glove boxes provide a physical barrier to isolate sensitive materials inside from environmental contamination or to protect the operator from the hazardous materials being manipulated. Are you in the market? Here's what you need to know...

Infographics 03-08-2016

Infographic: How to Safely Operate your Biosafety Cabinet

Best practices start with proper BSC selection, palcement and installation. Class II BSCs provide personal, product and environmental proteciton from biological hazards and aerosols, but airflow differs among types...

Infographics 12-08-2015

Infographic: The rundown-What type of water should I use in my application?

Using the right kind of water in your laboratory is important. To avoid wasted work, ruined results or sullied samples, make sure your laboratory is using water with the appropriate purity level for your particular application...

Infographics 11-03-2015

Biosafety Cabinets 101

What do you need from your BSC? Safety? Versatility? Comfort?

Infographics 11-17-2014

Infographic: A brand new kind of Biosafety Cabinet

The Type C1* is a biosafety cabinet unlike anything you've ever seen before. You'll have to see this to appreciate it...
*Type C1 pending definition by NSF/ANSI Standard 49

More News by Category

Switch to Desktop View

Login

Follow us:

Home | Products | News
Sales & Support | Contact

Phone: 816-333-8811 | Toll Free: 800-821-5525

© Labconco Corp. 2017 | Legal